Hello! I have one question that I have not been able to find an answer to.
If there are multiple networks with the MDEK1001 sensors using 4 anchors and 1 tag, would one network interfere with another causing more inaccuracies in the data?
Thanks.
Hello! I have one question that I have not been able to find an answer to.
If there are multiple networks with the MDEK1001 sensors using 4 anchors and 1 tag, would one network interfere with another causing more inaccuracies in the data?
Thanks.
Hi Yonda,
The network protocol in PANS 2.0 of MDEK1001 uses collision detection, avoidance and resolution. It allows the nodes to operate without collisions/interference as well as it can resolve the collisions when problem occurs. That is valid also for the independent networks that overlaps with each others.
The data between the networks are separated, but they do coexist with each others in a non-conflicting way.
Cheers,
TDK