Multi-iphone NI ranging on singular DWM3001CDK

Hi all,
First post here…
I’m currently working with a couple of DWM3001CDKs using the Qorvo NI Background app on iOS. I’ve confirmed that a single iPhone (17 pro running ios 27.0) can maintain background ranging sessions with two separate DWM3001CDKs simultaneously, which works well.

I’m now trying to understand the reverse scenario: supporting multiple iPhones with a single DWM3001CDK. (I could also just try my partner’s phone as well at the same time, but figured i’d ask the forum)

The intended application is indoor positioning, with several iPhones in proximity to a fixed UWB anchor. Each phone would have previously paired with the accessory and authorized background ranging. Ideally, when a phone returns within range, it would reconnect automatically, and the anchor could maintain or periodically schedule ranging sessions with multiple phones.

A few questions:

  1. Does the current QANI/NIQ firmware support multiple concurrent iPhone sessions on a single DW3110? I’ve seen some older discussions suggesting multiple BLE connections are possible, but that starting a second NI session can interrupt the first. Has this changed in newer SDK versions?
  2. Is it possible to time-multiplex ranging between multiple established NI sessions? I’m not looking for particularly high update rates per phone, so a round-robin approach would be perfectly acceptable.
  3. How tightly coupled is QANI’s BLE implementation to the UWB session management? I’m considering handling BLE connections and higher-level session scheduling on an external host (Jetson/Linux or a separate BLE MCU), while leaving the nRF52833/DW3110 responsible for UWB operations. Is there an existing interface for this, or would it require modifying the QANI application?

Ultimately, I’m trying to understand whether a single DWM3001CDK can reasonably service several previously enrolled iPhones in the background, without requiring a dedicated UWB radio for each phone.

Any pointers to the relevant SDK APIs, NIQ library versions, or existing examples would be appreciated.

Thanks!

I’m just another user, 1. but currently QANI is one phone per accessory. Once connected with BLE no other phone could discover the accessory. One could change the BLE design to allow multiple connections but the firmware design doesn’t share the UWB hardware across BLE sessions.,

The UCI firmware could run multiple downstream devices (controlee) from one accessory( as controller), but that is not QANI. But the dwm3001cdk only has one antenna and do cannot provide angle information.

  1. The BLE Oob communication is only used to pass a couple small messages to setup and end the UWB session. All the UWB content is handled by the UWB radios. So you could use some other comm mechanism to discover the accessory. The current QANI build doesn’t have any external comm other than BLE

2 I have no idea.

The phone does not pair with the accessory. At least in my application use I don’t experience any pairing requirement or possibility w the standard QANI interface.
I think pairing would make multi session harder

We have been able to modify the freeRTos hex file to track two (2) iPhones simultaneously.

Awesome!!
Thanks for sharing