Hi, everyone. I want to measure the Power Spectral Density [color=#333333]with a [/color][color=#333333]spectrum[/color][color=#333333] analyzer. I don’t know which code to use, the ex_04a_cont_wave [/color]
[color=#333333]or the ex_04b_cont_frame or anyone? I can’t understand the difference between them. [/color]
Here are two pictures, I use the [color=#333333]ex_04a_cont_wave and I measure the Power Spectral Density [color=#333333]with a [/color][color=#333333]spectrum[/color][color=#333333] analyzer. But the bandwidth is [/color][/color]
[color=#333333][color=#333333]113KHz and 2.2MHz. [color=#333333]Can someone help me out? Thanks a lot.[/color][/color][/color]
You’d need to use continuous frame mode for your spectrum test. 04a_cont_wave shall/could be used for crystal trim
This is explained in the IC user manual section 8 DW1000 Calibration.
The use of continuous mode is also highlighted in APS023 part 2 section 3.2 (page 6).
APS023 part 2 also describes the analyser setup.
Further more our IC datasheet shows the spectrums for all the channels
Latest revision IC user manual : rev 2.15
latest revision IC datasheet :rev 2.16
Available from: https://www.decawave.com/product-documentation/