[color=#333333]Hi,[/color]
[color=#333333]I have 4 MDEK1001 RTLS units. I have to get the accuracy 10cm in 200m line of sight for the autonomous vehicle in outdoors. [/color]
[color=#333333]Firstly, I do not know which criteria should I consider for the outdoor condition? [/color]
[color=#333333]Secondly, I have tested the accuracy in the indoor office ( [/color][color=#333333][size=large][font=Times]3.058 m x 3.114m) [/font][/size][/color][color=#333333]where I placed 3 anchors [/color][color=#333333][font=Times][size=large]at (0,0,2), (0,2.972,2), (3,2.972,2) coordinates. I have conducted several experiments to test the accuracy of the tag in different positions which gives around 10-13 cm accuracy. However, the ranging and consequently the position estimation missed and it becomes worse[/size][size=large] as I go further fro[/size][size=large]m the anchors. The refresh rate in 10 Hz which means it gives 10 position per second. I think that the issue might be[/size][size=large] the question of[/size][size=large] low power design[/size][size=large]. [/size][size=large]Is there any[/size][size=x-small] [/size][/font][/color][color=#333333][size=large][font=Times][color=#000000][size=medium]equations for calculating effective range given a transmitting power ?[/size][/color][/font][/size][/color]
[font=Times][color=#333333][color=#000000][size=large]Finally, How can I implement the kalman filtering to improve the accuracy on my tag? which hardware and software should I use to configure the tag? I mean by using those data (ranging and [/size][/color][size=medium]estimated[/size][color=#000000][size=large] position) which I have [/size][/color][/color][size=small][color=#000000]gotten[/color][/size][color=#333333][size=large][color=#333333] from the serial port on the Jlink ?[/color][/size][/color][/font]
[color=#333333][size=large][font=Times][color=#000000][size=medium]Anyone can help me?[/size][/color][/font][/size][/color]
[color=#333333][size=large][font=Times][color=#000000][size=medium]Thanks [/size][/color][/font][/size][/color]