[color=#222222][size=large][font=arial, sans-serif]Hello,[/font][/size][/color]
[color=#222222][size=large][font=arial, sans-serif]I need to have the location of a tag with a timestamp assigned to; for example, I need something like this tuple: (timestamp, location, tag ID). I have read from the MDEK1001 system user manual that I can see the location log either from a Bluetooth connection or from COM port of a PC. The provided example log file in the documentation which is also attached here shows the location of the tag in (x,y,z) form with the tag ID. As I see, there is not any timestamp in the log file. Is there any way to achieve location of a tag with a timestamp? If not, can I have the location log file either from PC or Bluetooth connection in real-time? In this way, I can combine the timestamp of the PC’s internal clock and the location log file programmatically and achieve the desired tuple![/font][/size][/color]
[color=#222222][size=large][font=arial, sans-serif]Thanks.[/font][/size][/color]