MDEK1001 not showing positions of tag or listener

I have setup of 4 anchors, 2 tags and 1 listener.
Listener is connected through usb to my mac. in minicom I did

 “nis 0x1234” to set the PanId and associate the bridge node with the network (0x1234 is only an example, the actual value may differ)
“nmb” 

this set it up as a listener where

dwm> si                                                                      
[011398.030 INF] sys: fw2 fw_ver=x01030001 cfg_ver=x00010700
[011398.030 INF] uwb0: panid=x09D9 addr=xDECAAF608B240189
[011398.040 INF] mode: bn (act,-)
[011398.040 INF] uwbmac: connected
[011398.040 INF] enc: off```

But on typing `les` or `lec` it gives nothing.
Also my anchors are positioned correctly as i could see tag positions in grid.

Any help is appreicated.

@eyshika
please dont post the same question into multiple topics.

Cheers
JK