I want to bring a few severe schematic editor UI limitations to the community’s and developers’ attention. While the back-end simulation math under the hood is excellent, the front-end layout engine currently features bugs that severely disrupt basic drafting throughput and waste engineering time.
1. Lack of Drag-Panning at Screen Borders (Invisible Walls)
When attempting to relocate components or text boxes across a large schematic, dragging an object to the edge of the viewport does absolutely nothing.
- In traditional CAD software (like LTspice), dragging an item past the border automatically auto-pans the canvas to create new space.
- In QSPICE, you slam into an invisible wall. The canvas position locks, forcing users to either zoom out completely or perform a clunky, multi-step “drop the part, drag the screen, pick up the part again” routine just to move items across a workspace.
2. Forced Schematic Window Shrinking Upon Simulation Runs
On a single-monitor setup, QSPICE violently overrides the user’s workspace preferences. When working with the schematic full-screen, hitting “Run Simulation” forces the waveform window to pop up while simultaneously shrinking the schematic window down (“Restore Down”).
- The Workflow Impact: This makes probing component currents or taking differential voltages across nodes nearly impossible because the component pins become tiny, shrunk targets.
- The Question: How do you permanently stop this automatic shrinking behavior? Why can’t QSPICE respect user-defined window sizes instead of forcing an unnecessary manual resizing step on every single run?
3. Slow and Jerky UI Re-rendering During Window Resizing
To add to the frustration of the forced shrinking issue, the interface is incredibly sluggish whenever you try to manually expand the schematic window back out to a readable full size to probe nodes.
- Resizing or tiling the window frame causes noticeable stuttering, lagging, and jerky re-rendering of the grid canvas.
- The custom drawing engine clearly struggles to cleanly handle dynamic window adjustments on standard desktop environments.
Usability and throughput are everything to working engineers. Forcing us to constantly fight screen boundaries and re-stretch scaled windows completely compromises the advantage of a fast solver. Please look into prioritizing standard window-state persistence and adding edge auto-panning to the layout editor.