Hi,
It is my understanding that there are three methods of logging data from the MDEK evaluation kit under its factory settings.
My configuration consists of [8 anchors and 4 tags] or [7 anchors, 4 tags, and 1 listener].
Method 1: PC logging connected to an active tag
positives: Timestamp from PC, ranges to best 4 anchors, and position relative to defined coordinate system
negative: Only receive data from connected tag, missing remaining 3 tags
Method 2: PC logging connected to a passive listener
positives: Timestamp from PC, position of all 4 tags
negative: No ranges are logged from the tags to the anchors
Method 3: Tablet logging via bluetooth
positives: Range and position for all 4 tags
negative: Timestamp seems to be relative to start-up of app, not time on the tablet
For my purposes I am looking to be able to log a useful timestamp, range to the best 4 anchors, and position for all 4 tags.
The way I see it there are two plausible solutions
- Replace the timestamp in the Android app to pull from the tablet’s clock
- Use the passive listener to obtain range data as well
I wanted to know if anyone would know how to do either one of these solutions or has figured out another way to obtain all of the data. Thanks!