I’d ideally like to obtain both position and distance from the tags in my network via one listener tag.
from the docs, I’m attempting to do this via the les, lec and lep commands. However, currently this only give me the position of the other tags (if the location engine on the listener is turned off) from which I recalculate the distances with respect to the anchor position.
With the location engine turned on on the listener, I only seem to get the distances to anchors of the listener tag, and not the other tags?
How does one obtain the anchor distances for active tags in the network via the listener?