Linear Y-axis with .AC analysis

Is there any way to set the Y-axis to linear, when showing .AC analysis result?

I am plotting the resistance with .plot V(out)/I(V1), but on the Y-axis setup I can only choose “Log” or “dB”. I want the values to show in Ohms, on a linear scale.
image

click log again, i.e. no selection in log or dB, and that is linear scale.

but linear scale is still magnitude and phase, no support to plot real and imagine in waveform viewer yet. Left y-axis is always abs() value in linear scale.

1 Like

Ah, thanks Kelvin! Works for me!