Hello All,
I’m currently working with the DW3220 module using the DW3_QM33_SDK_1.0.2, interfacing it with an nRF52832 over SPI.
So far, I have successfully:
- Established SPI communication
- Read the device ID of the DW3220
- Called
dwt_initialise()successfully (returnsDWT_SUCCESS)
However, when I call dwt_configure(), it fails and returns:
DWT_ERR_RX_CAL_PGF
I have tested both single-antenna and dual-antenna configurations, but the error persists in both cases.
Here is a summary of my setup:
- MCU: nRF52832
- UWB chip: DW3220
- SDK version: DW3_QM33_SDK_1.0.2
- Antenna configuration: tested both 1-antenna and 2-antenna setups
- Antennas: custom-made
I’ve attached images of the PCB and antennas below to help clarify the hardware setup.
My questions:
- What typically causes the
DWT_ERR_RX_CAL_PGFerror in this context? - Are there any specific hardware or antenna matching requirements for successful PGF calibration on DW3220?
- Is it possible to bypass PGF calibration (e.g., for initial bring-up or testing)?
- Are there any diagnostic tools or registers I can check to narrow down the root cause?
Looking forward to your suggestions.
Thank you!
Luc