Is the Bluetooth networking of the DWM1001 a mesh network?

  1. Is the Bluetooth networking of the DWM1001 a mesh network?
  2. Can I get data from any node in the same Bluetooth network through one of the anchor devices?
1 Like

Hi Jesse,

  1. No it is not a mesh network.

  2. No it is not possible, you can get data only from the node itself over BLE.

Please note MEDK/DWM1001 is demonstrating UWB rather than BLE. Having a BLE mesh would constraint the network and limit the performance that can be reach with UWB (i nterm of range for example)

Thanks
Yves