Hi I am using the DWM1001 kit in this configuration ( 2 tags at 5Hz update rate and 1 anchor which is the initiator ). I have been using serial uart to retrieve the anchor distances between each tags for my own application use. However, I have been receiving intermittent data loss from the serial uart port when both tags are running at the same time. I would receive no response from the serial port even after writing to get the anchor distances from the tag. This issue seems to be periodic where it happens for a few seconds after every minute. I do not have such issue when I am only running 1 tag 1 anchor.
Any idea if it could be a flaw caused by my setup?
Thanks