I use DWM3001C . My responder software not working with BLE and SD

Hi,

ı am using a dwm3001c that has a nrf52833 microprocessor. I want to set communication with initiator and responder . My initiator code that is ss_twr_initiator example in API.My responder code that is ss_twr_responder example in API. My initiator work werll with BLE and SD. ı add dfu and butonless and bluetooth com. to initiator.

But my responder not work with BLE and SD. I add dfu buttonless and bluetooth like initiator but not working. However only my adding code as ble buttonless and bluetooth work well . But this has not API as responder. AND API work well when that has not BLE and buttonless and bluetooth communication.

Please help me.

My responder as like following:

#define DEVICE_NAME “FY/Havelsan/RESPFY” /< Name of device. Will be included in the advertising data. */
#define APP_BLE_OBSERVER_PRIO 3 /
< Application’s BLE observer priority. You shouldn’t need to modify this value. */
#define APP_BLE_CONN_CFG_TAG 1 /< A tag identifying the SoftDevice BLE configuration. */
#define APP_ADV_INTERVAL 64 /
< The advertising interval (in units of 0.625 ms; this value corresponds to 40 ms). */
#define APP_ADV_DURATION BLE_GAP_ADV_TIMEOUT_GENERAL_UNLIMITED /< The advertising time-out (in units of seconds). When set to 0, we will never time out. */
#define MIN_CONN_INTERVAL MSEC_TO_UNITS(100, UNIT_1_25_MS) /
< Minimum acceptable connection interval (0.5 seconds). */
#define MAX_CONN_INTERVAL MSEC_TO_UNITS(200, UNIT_1_25_MS) /< Maximum acceptable connection interval (1 second). */
#define SLAVE_LATENCY 0 /
< Slave latency. */
#define CONN_SUP_TIMEOUT MSEC_TO_UNITS(4000, UNIT_10_MS) /< Connection supervisory time-out (4 seconds). */
#define FIRST_CONN_PARAMS_UPDATE_DELAY APP_TIMER_TICKS(20000) /
< Time from initiating event (connect or start of notification) to first time sd_ble_gap_conn_param_update is called (15 seconds). */
#define NEXT_CONN_PARAMS_UPDATE_DELAY APP_TIMER_TICKS(5000) /< Time between each call to sd_ble_gap_conn_param_update after the first call (5 seconds). */
#define MAX_CONN_PARAMS_UPDATE_COUNT 3 /
< Number of attempts before giving up the connection parameter negotiation. */
#define DEAD_BEEF 0xDEADBEEF /< Value used as error code on stack dump, can be used to identify stack location on stack unwind. */
#define MAX_TEST_DATA_BYTES (15U)
#define UART_TX_BUF_SIZE 256 /
< UART TX buffer size. */
#define UART_RX_BUF_SIZE 256
#define UNIT_TEST 0
#define SAMPLES_IN_BUFFER 5
#define UART_HWFC APP_UART_FLOW_CONTROL_DISABLED

static uint16_t m_conn_handle = BLE_CONN_HANDLE_INVALID; /< Handle of the current connection. */
static uint8_t m_adv_handle = BLE_GAP_ADV_SET_HANDLE_NOT_SET; /
< Advertising handle used to identify an advertising set. */
static uint8_t m_enc_advdata[BLE_GAP_ADV_SET_DATA_SIZE_MAX]; /< Buffer for storing an encoded advertising set. */
static uint8_t m_enc_scan_response_data[BLE_GAP_ADV_SET_DATA_SIZE_MAX]; /
< Buffer for storing an encoded scan data. */
static nrf_drv_uart_t m_uart = NRF_DRV_UART_INSTANCE(0);

static ble_gap_adv_data_t m_adv_data =
{
.adv_data =
{
.p_data = m_enc_advdata,
.len = BLE_GAP_ADV_SET_DATA_SIZE_MAX
},
.scan_rsp_data =
{
.p_data = m_enc_scan_response_data,
.len = BLE_GAP_ADV_SET_DATA_SIZE_MAX

}
};

static nrf_saadc_value_t m_buffer_pool[2][SAMPLES_IN_BUFFER];
static nrf_ppi_channel_t m_ppi_channel;
static uint32_t m_adc_evt_counter;

void wd_event_handler(void);
void wdt_init(void);

nrfx_wdt_channel_id m_channel_id;

NRF_BLE_GATT_DEF(m_gatt);
NRF_BLE_QWR_DEF(m_qwr);
BLE_CUS_DEF(m_cus);
BLE_ESS_DEF(p_ess);

APP_TIMER_DEF(m_notification_timer_id);
APP_TIMER_DEF(m_notification_timer_id_2);
APP_TIMER_DEF(m_app_timer_id);
APP_TIMER_DEF(m_timer);

extern ble_cus_t m_cus;
extern uint32_t ble_rate;
extern ble_ess_t p_ess;

extern example_ptr example_pointer;
extern int unit_test_main(void);
extern void build_examples(void);

void uart_error_handle(app_uart_evt_t * p_event)
{
if (p_event->evt_type == APP_UART_COMMUNICATION_ERROR)
{
//APP_ERROR_HANDLER(p_event->data.error_communication);
}
else if (p_event->evt_type == APP_UART_FIFO_ERROR)
{
APP_ERROR_HANDLER(p_event->data.error_code);
}

else if (p_event->evt_type == APP_UART_DATA_READY)
{
//app_uart_get(&a);
UNUSED_VARIABLE(app_uart_get(&a));
//printf(“%d”,a);
err_code=app_uart_put(a);
APP_ERROR_CHECK(err_code);

/err_code=app_uart_put(a);
APP_ERROR_CHECK(err_code);
/
}

else if (p_event->evt_type == APP_UART_TX_EMPTY)
{
//printf(“always_ok…”);
}

}

int main(void)
{

bool erase_bonds;

nrf_gpio_cfg_output(red_led);
nrf_gpio_cfg_output(green_led);
nrf_gpio_cfg_output(blue_led);
nrf_gpio_cfg_input(c_type_pin,NRF_GPIO_PIN_NOPULL);
nrf_gpio_cfg_input(bat_chg_v,NRF_GPIO_PIN_NOPULL);
nrf_gpio_cfg_input(user_buton, NRF_GPIO_PIN_PULLUP);

//nrf_gpio_cfg_input(ADC,NRF_GPIO_PIN_NOPULL);
nrf_gpio_pin_set(red_led);
nrf_gpio_pin_set(green_led);
nrf_gpio_pin_set(blue_led);

nrf_drv_clock_init();

nrf_drv_clock_lfclk_request(NULL);

wdt_init();

log_init();

// err_code = ble_dfu_buttonless_async_svci_init();
//APP_ERROR_CHECK(err_code);

timers_init();

power_management_init();

saadc_init();

ble_stack_init();

gap_params_init();

gatt_init();

qwr_init();

services_init();

advertising_init();

conn_params_init();

advertising_start();

uint32_t uart_enable;

if(!nrf_gpio_pin_read(bat_chg_v))
{
uart_enable= 15;
}
else
{
uart_enable= UART_PIN_DISCONNECTED;
}

const app_uart_comm_params_t comm_params =
{
RX_PIN_NUMBER,
TX_PIN_NUMBER,
RTS_PIN_NUMBER,
CTS_PIN_NUMBER,
UART_HWFC,
false,
#if defined (UART_PRESENT)
NRF_UART_BAUDRATE_115200
#else
NRF_UARTE_BAUDRATE_115200
#endif
};

APP_UART_FIFO_INIT(&comm_params,
UART_RX_BUF_SIZE,
UART_TX_BUF_SIZE,
uart_error_handle,
APP_IRQ_PRIORITY_LOWEST,
err_code);

APP_ERROR_CHECK(err_code);

build_examples();

gpio_init();

nrf52840_dk_spi_init();

dw_irq_init();

nrf_delay_ms(2);

if (UNIT_TEST)
{
unit_test_main();
}
else
{
example_pointer();
}

}

and my responder code as like following. Note this is same to original of API . I do not changed anything.

#include “deca_probe_interface.h”
#include <deca_device_api.h>
#include <deca_spi.h>
#include <example_selection.h>
#include <port.h>
#include <shared_defines.h>
#include <shared_functions.h>

#if defined(TEST_SS_TWR_RESPONDER)

extern void test_run_info(unsigned char *data);

/* Example application name */
#define APP_NAME “SS TWR RESP v1.0”

/* Default communication configuration. We use default non-STS DW mode. /
static dwt_config_t config = {
5, /
Channel number. /
DWT_PLEN_128, /
Preamble length. Used in TX only. /
DWT_PAC8, /
Preamble acquisition chunk size. Used in RX only. /
9, /
TX preamble code. Used in TX only. /
9, /
RX preamble code. Used in RX only. /
1, /
0 to use standard 8 symbol SFD, 1 to use non-standard 8 symbol, 2 for non-standard 16 symbol SFD and 3 for 4z 8 symbol SDF type /
DWT_BR_6M8, /
Data rate. /
DWT_PHRMODE_STD, /
PHY header mode. /
DWT_PHRRATE_STD, /
PHY header rate. /
(129 + 8 - 8), /
SFD timeout (preamble length + 1 + SFD length - PAC size). Used in RX only. /
DWT_STS_MODE_OFF, /
STS disabled /
DWT_STS_LEN_64, /
STS length see allowed values in Enum dwt_sts_lengths_e /
DWT_PDOA_M0 /
PDOA mode off */
};

/* Default antenna delay values for 64 MHz PRF. See NOTE 2 below. */
#define TX_ANT_DLY 16385
#define RX_ANT_DLY 16385

/* Frames used in the ranging process. See NOTE 3 below. /
static uint8_t rx_poll_msg[] = { 0x41, 0x88, 0, 0xCA, 0xDE, ‘W’, ‘A’, ‘V’, ‘E’, 0xE0, 0, 0 };
static uint8_t tx_resp_msg[] = { 0x41, 0x88, 0, 0xCA, 0xDE, ‘V’, ‘E’, ‘W’, ‘A’, 0xE1, 0, 0, 0, 0, 0, 0, 0, 0, 0, 0 };
/
Length of the common part of the message (up to and including the function code, see NOTE 3 below). /
#define ALL_MSG_COMMON_LEN 10
/
Index to access some of the fields in the frames involved in the process. /
#define ALL_MSG_SN_IDX 2
#define RESP_MSG_POLL_RX_TS_IDX 10
#define RESP_MSG_RESP_TX_TS_IDX 14
#define RESP_MSG_TS_LEN 4
/
Frame sequence number, incremented after each transmission. */
static uint8_t frame_seq_nb = 0;

/* Buffer to store received messages.

  • Its size is adjusted to longest frame that this example code is supposed to handle. */
    #define RX_BUF_LEN 12 // Must be less than FRAME_LEN_MAX_EX
    static uint8_t rx_buffer[RX_BUF_LEN];

/* Hold copy of status register state here for reference so that it can be examined at a debug breakpoint. */
static uint32_t status_reg = 0;

/* Delay between frames, in UWB microseconds. See NOTE 1 below. */
#define POLL_RX_TO_RESP_TX_DLY_UUS 650

/* Timestamps of frames transmission/reception. */
static uint64_t poll_rx_ts;
static uint64_t resp_tx_ts;

/* Values for the PG_DELAY and TX_POWER registers reflect the bandwidth and power of the spectrum at the current

  • temperature. These values can be calibrated prior to taking reference measurements. See NOTE 5 below. */
    extern dwt_txconfig_t txconfig_options;

/*! ------------------------------------------------------------------------------------------------------------------

  • @fn main()
  • @brief Application entry point.
  • @param none
  • @return none
    /
    int ss_twr_responder(void)
    {
    /
    Display application name on LCD. */
    //test_run_info((unsigned char *)APP_NAME);

/* Configure SPI rate, DW3000 supports up to 36 MHz */
port_set_dw_ic_spi_fastrate();

/* Reset and initialize DW chip. /
reset_DWIC(); /
Target specific drive of RSTn line into DW3000 low for a period. */

Sleep(2); // Time needed for DW3000 to start up (transition from INIT_RC to IDLE_RC, or could wait for SPIRDY event)

/* Probe for the correct device driver. */
dwt_probe((struct dwt_probe_s *)&dw3000_probe_interf);

while (!dwt_checkidlerc()) /* Need to make sure DW IC is in IDLE_RC before proceeding */ { };
if (dwt_initialise(DWT_DW_INIT) == DWT_ERROR)
{
//test_run_info((unsigned char *)"INIT FAILED ");
//while (1) { };
}

/* Enabling LEDs here for debug so that for each TX the D1 LED will flash on DW3000 red eval-shield boards. */
dwt_setleds(DWT_LEDS_ENABLE | DWT_LEDS_INIT_BLINK);

/* Configure DW IC. See NOTE 13 below. /
/
if the dwt_configure returns DWT_ERROR either the PLL or RX calibration has failed the host should reset the device */
if (dwt_configure(&config))
{
// test_run_info((unsigned char *)"CONFIG FAILED ");
//while (1) { };
}

/* Configure the TX spectrum parameters (power, PG delay and PG count) */
dwt_configuretxrf(&txconfig_options);

/* Apply default antenna delay value. See NOTE 2 below. */
dwt_setrxantennadelay(RX_ANT_DLY);
dwt_settxantennadelay(TX_ANT_DLY);

/* Next can enable TX/RX states output on GPIOs 5 and 6 to help debug, and also TX/RX LEDs

  • Note, in real low power applications the LEDs should not be used. */
    dwt_setlnapamode(DWT_LNA_ENABLE | DWT_PA_ENABLE);

/* Loop forever responding to ranging requests. /
while (1)
{
/
Activate reception immediately. */
dwt_rxenable(DWT_START_RX_IMMEDIATE);

/* Poll for reception of a frame or error/timeout. See NOTE 6 below. */
waitforsysstatus(&status_reg, NULL, (DWT_INT_RXFCG_BIT_MASK | SYS_STATUS_ALL_RX_ERR), 0);

if (status_reg & DWT_INT_RXFCG_BIT_MASK)
{
uint16_t frame_len;

/* Clear good RX frame event in the DW IC status register. */
dwt_writesysstatuslo(DWT_INT_RXFCG_BIT_MASK);

/* A frame has been received, read it into the local buffer. */
frame_len = dwt_getframelength();
if (frame_len <= sizeof(rx_buffer))
{
dwt_readrxdata(rx_buffer, frame_len, 0);

/* Check that the frame is a poll sent by “SS TWR initiator” example.

  • As the sequence number field of the frame is not relevant, it is cleared to simplify the validation of the frame. */
    rx_buffer[ALL_MSG_SN_IDX] = 0;
    if (memcmp(rx_buffer, rx_poll_msg, ALL_MSG_COMMON_LEN) == 0)
    {
    uint32_t resp_tx_time;
    int ret;

/* Retrieve poll reception timestamp. */
poll_rx_ts = get_rx_timestamp_u64();

/* Compute response message transmission time. See NOTE 7 below. */
resp_tx_time = (poll_rx_ts + (POLL_RX_TO_RESP_TX_DLY_UUS * UUS_TO_DWT_TIME)) >> 8;
dwt_setdelayedtrxtime(resp_tx_time);

/* Response TX timestamp is the transmission time we programmed plus the antenna delay. */
resp_tx_ts = (((uint64_t)(resp_tx_time & 0xFFFFFFFEUL)) << 8) + TX_ANT_DLY;

/* Write all timestamps in the final message. See NOTE 8 below. */
resp_msg_set_ts(&tx_resp_msg[RESP_MSG_POLL_RX_TS_IDX], poll_rx_ts);
resp_msg_set_ts(&tx_resp_msg[RESP_MSG_RESP_TX_TS_IDX], resp_tx_ts);

/* Write and send the response message. See NOTE 9 below. /
tx_resp_msg[ALL_MSG_SN_IDX] = frame_seq_nb;
dwt_writetxdata(sizeof(tx_resp_msg), tx_resp_msg, 0); /
Zero offset in TX buffer. /
dwt_writetxfctrl(sizeof(tx_resp_msg), 0, 1); /
Zero offset in TX buffer, ranging. */
ret = dwt_starttx(DWT_START_TX_DELAYED);

/* If dwt_starttx() returns an error, abandon this ranging exchange and proceed to the next one. See NOTE 10 below. /
if (ret == DWT_SUCCESS)
{
/
Poll DW IC until TX frame sent event set. See NOTE 6 below. */
waitforsysstatus(NULL, NULL, DWT_INT_TXFRS_BIT_MASK, 0);

/* Clear TXFRS event. */
dwt_writesysstatuslo(DWT_INT_TXFRS_BIT_MASK);

/* Increment frame sequence number after transmission of the poll message (modulo 256). /
frame_seq_nb++;
}
}
}
}
else
{
/
Clear RX error events in the DW IC status register. */
dwt_writesysstatuslo(SYS_STATUS_ALL_RX_ERR);
}
}
}
#endif

My responder code when I download ,ıt communicate with initiator for 5 times then crash and not communicate.

Preprocessors definitions:

but only API can full communicate.

BL_SETTINGS_ACCESS_ONLY

NRF_DFU_TRANSPORT_BLE=1

BOARD_DWM3001C

CONFIG_GPIO_AS_PINRESET

FLOAT_ABI_HARD

NO_VTOR_CONFIG

INITIALIZE_USER_SECTIONS

NRF52833_XXAA

NRF_SD_BLE_API_VERSION=7

S140

SOFTDEVICE_PRESENT

Hi,
I contact to nrf on another topic((+) SOFTDEVICE: INVALID MEMORY ACCESS - Nordic Q&A - Nordic DevZone - Nordic DevZone (nordicsemi.com)). then

Now statues is;

but ı change from *((volatile uint32_t *)0x40000E00) = m_anomaly_198_preserved_value; to *((volatile uint32_t *)0x40002000) = m_anomaly_198_preserved_value; in anomaly_198_disable and enable now not crash my responder continues advertise but dwm3001c module that has a responder code can not receive frame .

responder can frame only one time in 15-20 loop.

but if ı do not use SD AND BLE , my RESPONDER CAN RECEİVE FRAME WELL.

now how can I fix to receive frame issue?

ı found reason to can not receive frame on responder.

this issue is that responder wait for long time on waitforsysstatus(NULL, NULL, DWT_INT_TXFRS_BIT_MASK, 0);

then

responder can not receive.

this function’s define is:

please help me.

I can not find reason.I can not debug step by step .Because I have softdevice.