Hello -
Im wondering if there is API support for the on-board GPIO to send status over BLE to another DWM1001 module (acting as master in piconet network)?
My system consists of 1 tag which will take in GPIO to get some switch inputs from a user, then share the state of the GPIO with a host BLE module (another DWM1001 acting as an anchor). As a side note, there will be 2 anchor nodes for localization. The one receiving the Bluetooth data from the Tag node will be sending coordinates of the tag over SPI or UART to an external host controller (i.e. Linux box, RaspberryPi, etc.)
Can this be done over BLE? I do not see any mention of GPIO access on the DWM1001-Bluetooth-API pdf.
Thanks!