Hi,
I want to obtain data using listener node over ethernet using uart to ethernet USR .
When i am sending Double Enter on terminal (telnet) then it is showing @ sign.
That is i am not able to switch to shell mode of uart to send commands to listener node.
Is it possible to obtain data from listener node over ethernet without using gateway?
If possible then what i need to do?
Please suggest me
Thanks
Akansha
Hi Akansa,
There is no ethernet interface or api on the dwm1001 module, so I’m not sure what you want to achieve exactly. The module interfaces are UART, SPI and BLE.
Using one or multiple gateways (raspberry pi 3b + dwm1001-dev) in the network adds connectivity between gateway nodes over ethernet and wifi.
Hope it helps,
Yves
Hi,
I got the mistake
Thanks
Akansha