Gateway with dwm-daemon on Raspberry pi

Hi All,

can you please provide more details about the issue?

  1. Which Raspberry hardware revision are you using? If possible please send a picture of the Raspberry with the DWM1001.
  2. Is the DWM1001 reflashed with the R2 binary?
  3. Which Raspberry Image are you using? The official one from the Release 2?
  4. How do you start the DWM Daemon? Manually or just restarted the Raspberry?
  5. Can you get the system working or it keeps failing like this?
  6. Can you enter the module shell using: minicom -D /dev/serial0 (and double enter)?
  7. Please send outputs of the commands on the failing system:
    1. lsmod
    2. ls -la /dev/dwm0
    3. ps ax | grep dwm

Thanks!
Cheers, TDK