First path index understanding

Time of flight is not calculated from CIR directly, but calculated using the timestamps of message TX and RX.

In the case of ToF, CIR (and other diagnostic data) can be used to determine if the ToF calculation is reliable or not. For example, you can see (guess) if it is a LOS or NLOS scenario and then adjust or discard your ToF calculation based on the diagnostic data.

It is normal that the FP indices are mostly between 730 and 750. FP index serves as a reference point for multipath component analysis rather than an absolute value which is proportional to ToF. In the CIR plot, you can see multiple peaks except for the peak of LOS. They correspond to multipath components caused by reflections, scatterings or diffractions. By checking the index difference between these peaks wrt the first path, you can roughly calculate the path difference between these multipath components and the first path, though it is not crucial information for LOS ranging.