testsignal.csv (155.9 KB)
Somehow the fft result of my testsignal is not plausible (see figure).
You surely have a lot on the plate, but additionally, I stumbled upon a few issues that could use a look when you have some time:
• Linear scale ticks: The tick size on the frequency scale currently isn’t adjustable when logarithmic is unselected.
• DFT vs. True FFT: The dropdown currently uses numbers that lead to a DFT. Switching to power-of-two point numbers would be a huge help to ensure a true FFT. It also would improve the UX since selecting numbers with a long row of zeros from a dropdown menu is a bit clunky.
• Point doubling: The chosen point number is doubled in the background. I see the intention but it’s a bit confusing.
Appreciate your time and effort on this!