Feature Request: Minimum and Maximum Cursor functions that apply to a zoomed plot window

@Engelhardt ,

I have a simple feature request.

When using cursors in a zoomed plot window, I execute the “Minimum” and “Maximum” math operations on each cursor. The “Minimum” operation forces the cursor the the FIRST minimum value in the entire dataset. This is true even if in the case of the zoomed window when the FIRST min value is off-window.

This above is also true of the “Maximum” math operation.

It would be preferred to find the FIRST minimum or maximum value of the displayed section of the plotted wave. Right now I have to manually move the cursor.

Strangely, the other math operations such as Average, Peak To Peak, RMS and Integrate operate between the cursors which is a desired feature.

Thank you for your consideration.

Len