Hi, I am using DWM3001CDK for a project. I am new to the UWB ranging. I tried to flash the “\Qorvo_Nearby_Interaction_3_2_1\Software\Accessory\Binaries\DWM3001CDK-QANI-FreeRTOS_full_QNI_3_0_0.hex” using JLink. but as soon as I enter “go” it shows me the error “Memory map ‘after startup completion point’ is active” and I see solid red light on the board. I also can not see any device on Qorvo Nearby Interaction app on my iphone. Can somebody please help me? Thanks!
Here is the details of command i used:
J-Link>loadfile “O:\Qorvo_Nearby_Interaction_3_2_1\Software\Accessory\Binaries\DWM3001CDK-QANI-FreeRTOS_full_QNI_3_0_0.hex”
‘loadfile’: Performing implicit reset & halt of MCU.
Memory map ‘before startup completion point’ is active
Reset: Halt core after reset via DEMCR.VC_CORERESET.
Reset: Reset device via AIRCR.SYSRESETREQ.
Downloading file [O:\Qorvo_Nearby_Interaction_3_2_1\Software\Accessory\Binaries\DWM3001CDK-QANI-FreeRTOS_full_QNI_3_0_0.hex]…
J-Link: Flash download: Bank 0 @ 0x00000000: 1 range affected (4096 bytes)
J-Link: Flash download: Total: 0.779s (Prepare: 0.124s, Compare: 0.414s, Erase: 0.092s, Program & Verify: 0.053s, Restore: 0.093s)
J-Link: Flash download: Program & Verify speed: 75 KB/s
O.K.
J-Link>r
Reset delay: 0 ms
Reset type NORMAL: Resets core & peripherals via SYSRESETREQ & VECTRESET bit.
Reset: Halt core after reset via DEMCR.VC_CORERESET.
Reset: Reset device via AIRCR.SYSRESETREQ.
J-Link>g
Memory map ‘after startup completion point’ is active