I’ve got two DWM3001CDK boards and trying to configure them with BPRF set 3 (SP1) using “initf 3” and “respf 3”. But both devices are returning errors.
They do work in other modes such as BPRF set 4 using “initf 4” and “respf 4”.
I think they should not work, because initf/respf referred to the “deferred ds-twr” as specked in fira. In that mode the ranging frames are always either Bprf 4 (sfd 4z) or bprf 6 (sfd 4a).