Hi @akash,
Thanks for responding, I have followed that tutorial and I am receiving distances from all 4 anchors.
My issue is that I am receiving the distances asynchronously and at a slower frequency than I would expect. Using the CLI I set the SLOT=2400, BLOCK=192, ROUND=24 and RRU=DSTWRNDEF. Which, if I’m not mistaken, should result in a frequency around 20 Hz. Instead I am receiving distance results at about 6 Hz.
I have seen reference in other answers DW3000 limitations and frequency adjustment - #2 by Wassim_Qorvo to delay variables that may be the cause but have been unable to locate them within the SDK.
Any help with locating these delays or with finding another solution to my problem would be appreciated.
Regards,
Cael