Hello,
I currently have a DWM3000 EVB + Nucleo F429ZI (STM32CubeIDE) , and have previously worked with the DWS1000 board for the DWM1000 modules. I have a question regarding setting up the api.
Here is what I have tried so far
- Followed the instructions in the power point presentation attached to the API (but cant really find the .elf) file specified.
- Tried including the linked libraries and the other api files, compiles without an issue, but the dwt_probe function returns DWT_ERROR (a value of -1, and all subsequent commands end up throwing hard faults)
The peripherals were initiated using STM32 Cube MX ( configuration almost identical to the one provided with the examples) and the code used was the ex00a_reading_dev_id one. The API was sourced from qorvos website (DW3xxx_QM33_CR6.0C)
Any help would be appreciated!
Thanks!