I’ve been looking through the available documentation but can’t find information on which nRF52832 pins are used for SPI communication with DW1000 and which for I2C for accelerometer. I am experimenting with already existing firmware for nRF52832 + DWM1000 and trying to run it on DWM1001 but without this information it’s more difficult. I would greatly appreciate if somebody could help me with figuring this out or pointing to correct documentation.
Hi!
I’ve been reading the schematics but I don’t find where are connected some pins.
For instance, P0.02, P0.04, P0.04 are connected to the label J6,J7 and J8 but they are never used,
Are they accessible ? They don’t appear in the pinout of the module