I want to get distance only between several Tags and 2 Anchors using UART generic mode.
From reading the Api Guide it appears I need to do the following, is this correct?
Set up the 2 Anchors, One must be set as Initiator
Host Disables Location Engine by sending “cfg_tag_set” command (0x0x) with “loc_engine_en = 0”
LOOP
Host reads distance to anchors using “dwm_log_get” command (0x0C) and reads TLV type 0x49 from received packet
Delay between calling function = ???
I notice when I look at the “Shell Mode” version of the command (“les”) it states that "sending this command multiple times will turn on/off this functionality.
Does this only apply to the shell version of the command?