Guys. I see several questions about DWM1001 range but seems that still an open question.
For the LOS environment I need transmission power . Is it -17dBm ?
Also, I see in antenna manual that antenna gain varies with direction. So in order to calculate the distance, shall I use the worst case scenario for 6.5GHz acoording to figure 2D radiation pattern or the average value (-1.1db)?
Using these parameters in a FRIIS calculator, I get the following power receptions:
25 meters -96.35 dBm
50 meters - 102.4 dBm
These values are quite close to Tx speed 6.8 Mbps and 110 Kbps.
I see some comments here wich shows ranges between 100m and 330 meters but seems that are not according to results obtained by FRIIS calculator and is closer to some other reports seen here in this forum.
Which are really correct ?