Hi Yves,
Thanks for the reply. Here is the result of “si” command. This is just after turning on the device. If you need the result after the issue I have to keep it running till it happens.
Best regards,
Arash
==========================
dwm> si
[000023.890 INF] cfg:
[000023.890 INF] >fw2=x00044000
[000023.890 INF] board=DWM1001_A2
[000023.890 INF] cfg_ver=x00010700
[000023.900 INF] fw_ver=x01010501
[000023.900 INF] hw_ver=xDECA002A
[000023.900 INF] opt=x13C1A340
[000023.910 INF] fw_size[0]=x0001F000
[000023.910 INF] fw_size[1]=x00022000
[000023.910 INF] fw_size[2]=x0003C000
[000023.920 INF] fw_csum[0]=x9445F89E
[000023.920 INF] fw_csum[1]=x36D9BFF1
[000023.930 INF] fw_csum[2]=x222552AD
[000023.930 INF] opt: ACC LEDS PASV TWR LE BPC UWB0 BLE I2C SPI UART
[000023.940 INF] mcu: temp=22.5 hfclk=xtal:on lfclk=rc:on
[000023.940 INF] uptime: 00:00:23.940 0 days (23940 ms)
[000023.950 INF] mem: free=3424 alloc=11680 tot=15104
[000023.950 INF] uwb: ch5 prf64 plen128 pac8 txcode9 rxcode9 sfd0 baud6800 phrex t sfdto129 smart1
[000023.960 INF] uwb: tx_pwr=xC5/x2B4B6B8B 125:250:500:norm[ms]=20:17:14:11[dB] pgcnt=713 temp=13
[000023.970 INF] uwb0: lna=0 xtaltrim=27 tx_delay=16472 rx_delay=16472
[000023.980 INF] uwb0: ID dev=xDECA0130 part=xC4B49C21 lot=x013A6102
[000023.990 INF] uwb0: panid=xB5A6 addr=xDECA8734B5449C21
[000023.990 INF] mode: tn (pasv,twr,np,le)
[000024.000 INF] uwbmac: disconnected
[000024.000 INF] ble: addr=D1:F5:C2:1A:55:CA
dwm>
====================================
UPDATE:
After about 1.5 hours I received the error. Here is the “lec” output when error occurs and the result of “si” after that:
[005199.680 INF] uwb: tdma (not synced)
[005199.680 INF] uwb: reinit
[005219.340 INF] uwb: tdma (synced)
POS,0,1698,27.54,4.24,0.90,50,xDC
POS,0,0000,0.00,0.00,0.00,0,x00
POS,0,0000,0.00,0.00,0.00,0,x00
POS,0,0000,0.00,0.00,0.00,0,x00
POS,0,0000,0.00,0.00,0.00,0,x00
POS,0,0000,0.00,0.00,0.00,0,x00
POS,0,0000,0.00,0.00,0.00,0,x00
POS,0,0000,0.00,0.00,0.00,0,x00
POS,0,0000,0.00,0.00,0.00,0,x00
POS,0,0000,0.00,0.00,0.00,0,x00
POS,0,0000,0.00,0.00,0.00,0,x00
POS,0,0000,0.00,0.00,0.00,0,x00
POS,0,0000,0.00,0.00,0.00,0,x00
POS,0,0000,0.00,0.00,0.00,0,x00
POS,0,0000,0.00,0.00,0.00,0,x00
POS,0,0000,0.00,0.00,0.00,0,x00
POS,0,0000,0.00,0.00,0.00,0,x00
POS,0,0000,0.00,0.00,0.00,0,x00
POS,0,0000,0.00,0.00,0.00,0,x00
POS,0,0000,0.00,0.00,0.00,0,x00
POS,0,0000,0.00,0.00,0.00,0,x00
POS,0,0000,0.00,0.00,0.00,0,x00
POS,0,0000,0.00,0.00,0.00,0,x00
POS,0,0000,0.00,0.00,0.00,0,x00
POS,0,0000,0.00,0.00,0.00,0,x00
assertion “0 != p_ble_evt” failed: file “/virtual/projects/leaps/git/910-argo/src/lib/ble/ble-server.c”, line 2212, function: ble_server_on_ble_evt
app_error_print():
Fault identifier: 0x4001
Program counter: 0x0
Fault information: 0x2000AE6C
Line Number: 38
File Name: /virtual/projects/leaps/git/910-argo/src/ecos/lib/ble/process-ble.c
Error Code: 0x1
DWM1001 TWR Real Time Location System
Copyright : 2016-2017 LEAPS and Decawave
License : Please visit https://decawave.com/dwm1001_license
Compiled : Nov 20 2017 12:51:26
Help : ? or help
dwm> si
[000285.130 INF] cfg:
[000285.130 INF] >fw2=x00044000
[000285.130 INF] board=DWM1001_A2
[000285.140 INF] cfg_ver=x00010700
[000285.140 INF] fw_ver=x01010501
[000285.140 INF] hw_ver=xDECA002A
[000285.150 INF] opt=x13C1A340
[000285.150 INF] fw_size[0]=x0001F000
[000285.150 INF] fw_size[1]=x00022000
[000285.160 INF] fw_size[2]=x0003C000
[000285.160 INF] fw_csum[0]=x9445F89E
[000285.160 INF] fw_csum[1]=x36D9BFF1
[000285.170 INF] fw_csum[2]=x222552AD
[000285.170 INF] opt: ACC LEDS PASV TWR LE BPC UWB0 BLE I2C SPI UART
[000285.180 INF] mcu: temp=26.5 hfclk=xtal:on lfclk=rc:on
[000285.180 INF] uptime: 00:04:45.180 0 days (285180 ms)
[000285.190 INF] mem: free=3424 alloc=11680 tot=15104
[000285.190 INF] uwb: ch5 prf64 plen128 pac8 txcode9 rxcode9 sfd0 baud6800 phrext sfdto129 smart1
[000285.200 INF] uwb: tx_pwr=xC4/x2B4B6B8B 125:250:500:norm[ms]=20:17:14:11[dB] pgcnt=713 temp=13
[000285.210 INF] uwb0: lna=0 xtaltrim=27 tx_delay=16472 rx_delay=16472
[000285.220 INF] uwb0: ID dev=xDECA0130 part=xC4B49C21 lot=x013A6102
[000285.230 INF] uwb0: panid=xB5A6 addr=xDECA8734B5449C21
[000285.230 INF] mode: tn (pasv,twr,np,le)
[000285.240 INF] uwbmac: disconnected
[000285.240 INF] ble: addr=D1:F5:C2:1A:55:CA
dwm>