Hello,
The DWM1001-Dev Board has it’s own “Localization Unit” (using the maximum likelihood estimation) to get the x,y,z coordinates from the position of the tag.
The API provides access to the position, is it possible to use this position as input for a Kalmanfilter to generate a Tracking System(moving objects) or is this allready implemented?
I think the maximum likelihood estimation is only used to generate the position of a not moving object. The Kalmanfilter is used to smooth position information of an moving object to generate a motion path.
Thanks for help