You will have to ask Decawave as I don’t speak for them.
I will note that the FCC rules for UWB get more complex for the lower bands. 15.517 requires use only “indoors” and 15.519 requires use only for “hand held” devices, and perhaps neither of which can be assured for the DWM1001 on which the MDEK is based.
If certifying under 15.250, the rule the DWM1001 is certified under presently, and you go to a lower band, you have to be under -51.3 dBm/Mhz EIRP. This is a 10 dB penalty in power which will reduce your range to about 30-50% of what it was before. This assumes the antenna on a DWM1001 actually works well at lower bands, which I don’t think it does. I don’t think Decawave tested it for the lower bands under 15.250 in any case, so there’s no regulatory basis for doing that.
If you certify under 15.517 or 15.519, then you can use -41.3 dBm/MHz EIRP. But you have to abide by the use limitations (indoors, or handheld). I don’t think Decawave certified the DWM1001 under 15.517 or 15.519. That could happen in the future, though.
I am not directly familiar with the Brazil rules for UWB.
This is a complex subject I have written about previously:
Unlike most radio rules, UWB has use case limitations. Anchors mounted outdoors which transmit are in a gray area. Any truly usable UWB system has one or more fixed transmitters somewhere.
Mike Ciholas, President, Ciholas, Inc
3700 Bell Road, Newburgh, IN 47630 USA
mikec@ciholas.com
+1 812 962 9408