Hi All,
I am trying to test DW3000 PDoA KIT with following condition.
- Distance between DW3120 (Anchor) and DW3110 (Tag) is fixed to 1M. (Calibration is OK.)
- Checked the accuracy of angle by rotating the DW3120 (Anchor) only.
- When DW3120 (Anchor) makes angle (0°, -15°, -30°, -45°) with DW3110 (Tag),
I can get the test results with very small error of angle. - When DW3120 (Anchor) makes angle (0°, +15°, +30°, +45°) with DW3110 (Tag),
I can get the test results with bigger error of angle than test results of (-)angle.
I would like to get a better performance for (+)angle than now.
Please advise me what to do.
Thanks.