hi,
i am using DW1001 development kit. i tried some of the combination to test the Decawave kit, it works fine, as per my understand the Decawave kit have STM32(MCU), NRF53832,DW1000.
can we write the code into NRF52832 as bluetooth and main controller(instead of STM32), if it is possible can anyone have the driver code for NRF52832.
Hii
I am glad to help you .Yes, ofcourse it is possible to write a code for the NRF52832 to serve as both a Bluetooth module and main controller instead of used the STM32. You want need to develop firmware that integrates Bluetooth functionality and handles the main controller tasks. The NRF52832 supports Bluetooth Low Energy (BLE) and can a function as a standalone microcontroller. However, you will need to ensure that your compatibility with the DW1000 and develop or find appropriate driver code for it. You can also search online for NRF52832 driver libraries or refer to documentation provided by the chip manufacturer. Additionally, community forums or developer communities related to the NRF52832 may offer support or resources form integrating the DW1000.