Hi,
So i have a problem where I get range values between the a tag and an anchor for example:
RANGE = [16,15,16,15,16,15,16,15]
I do not change the distance between the anchor and tags the only thing that I do is reboot the anchor and the values change:
RANGE= [18,19,18,19,18,19,18,19]
The fact that it constantly changes is a problem because it means every time i have to recalibrate the values. Does anyone have any idea as to why this happens?
Also should I ground every single Vss pin or if one Vss pin is it fine since they all interconnected?