Default value for capacitor instance initial condition

Thank you @KSKelvin for the explanation.

Interestingly, for the inductor the default value of IC is “none” (matching your suggestion) while for the capacitor it is “0.0”.

Also, I found this reply from Mike Engelhardt from July 2023 talking about the use of the UIC option of the .tran command

If the UIC option is used, what ICs will be used for the components without explicitly defined ICs? Will the defaults be used - “none” for inductors and “0.0” for capacitors?