I could setup the following scenario but it would take quite some time, so I thought I would throw this out.
Using the DWM1001 module, if
[list]
[]I provide three anchors all within range of each other and all belonging to the same network, alpha.
[]I provide a second set of three anchors again belonging to alpha but well out of range of the first set of three.
[]The two segments are far apart from each other, 200 m, for example.
[]I provide a tag that can move freely between the two segments.
[/list]
The segments may be referenced (x,y,z) to each other but not know the other exists.
Of course, the tag won’t know where it is outside of the segments.