I want to use DWM1001 with the lowest update rate for a stationary object localization. Which configuration would help me to make it the least power hungry device and also I want to last the battery for 1 year.
I did test the DWM1001 mounted on dev kit. Power consumption is surprisingly low (~30mA). If you do stationary detection, i believe it will further reduce the consumption on the tags.
For the system to last 1 year, you must use deep sleep function as well when the device is not in use.
Read System Overview. I have not tried it on this processor but other processors work great with deep sleep. Plus the documentation talks about it as well.