Annoying quirk in QSpice auto-zoom

I have simulations where I seek a null.
QSpice works well, for modest nulls, but as things improve it fails to Auto-zoom, instead falls back to a zoomed-out flat line, this default choice looks about 200uV/div in 1V.
I am forced to manually zoom in every time, with multiple box-drags to see the actual plot.

It looks like the code tried to scale, and if it cannot reach a sizable screen %, it instead serves up the SW chosen default.

That seems a strange decision, zoom-to-fit should do what it says, and do the best it can, even if that max zoom is not over 50% of screen height.

Having a strange fall-back to zoom-out simply wastes time.

Here is a manually zoomed good-null case. - yes, it is sub uV, but QSpice should be able to zoom to that, if I can do it manually.