Hello All!
I am creating an app separate from the decawave mobile app for my company and I want to be able to get the anchor positions that are stored on the devices from the following characteristic via the decawave bluetooth api doc:
f0f26c9b-2c8c-49ac-ab60-fe03def1b40c
Persisted
position
13
bytes
X,Y,Z coordinates each 4-byte
precision + quality factor (1 byte,
value 1 - 100)
Taking decoding errors out of the equations, when I do a read characteristic command I get back an empty byte array instead of a 13 byte array. The position shows up correctly in the decawave app. Are there special permissions that I need to get this value?
Thanks!
Derek