Anchor capacity

Also how can I know the maximum processing capacity of an anchor x number of tags x payload size ?

Also the same question to anchors which a closer to the gateway ?

Hi Nudel,

I guess you are using DWM1001 based devices and PANS software library ?

If that’s correct, please refer to the DWM1001 system architecture and performance guide. The capacity metric is not per anchor. The payload size is fixed in the system. Similarly the proximity between anchor and gateway does not impact capacity.

PANS contains 30 anchors seats and 150Hz capacity for location (so 15 tags at 10Hz for example).

Thanks
Yves